Unable to remove constraints from a projected point in a sketch

2021-10-06T23:27:07Z

Summary


Details

Having used the Sketch Project Curve command to project the arc center of a hole in another part to a sketch, it is not possible to move the projected point.  NX raises the message: "One or more constraints are violated with the selected motion type.  Remove some constraints, change the motion type or change the object selection".  How do you find and delete the constraints that are preventing the point from being moved?

Solution

Double-click the projected point and uncheck "Associative" from the Settings block of the dialog and OK the change. The point can then be moved.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V1859
Function: SKETCHER

Ref: 002-7004591

KB Article ID# PL7004591

Contents

SummaryDetails

Associated Components