How to export all edges as wireframe to IGES

2021-10-06T23:27:17Z

Summary


Details

How to export all edges of a model as wireframe curves to an IGES file.

Solution

 1. EDIT THE "UGII_BASE_DIR\IGES\igesexport.def" FILE 
 a. Open the "UGII_BASE_DIR\IGES\igesexport.def" file in a text editor. 
 b. Add the option, 'All Solid Edges', to the UGI_CURVE_MASK line so it 
 looks like the entry below: 
 UGI_CURVE_MASK = Points,Lines,Arcs,Conics,Rational B-Spline 
 Curves,Solid Edges on Drawings,All Solid Edges 
 c. Remove all the values for the UGI_SURF_MASK and UGI_SOLID_MASK options: 
 UGI_SURF_MASK = 
 UGI_SOLID_MASK = 
 d. 'Save As' this file to UGII_BASE_DIR\IGES\igesexport_wireframe.def


2. USE THIS SETTINGS FILE WHEN EXPORTING 
 a. In NX, select 'File-->Export-->IGES'. 
 b. On the 'Files' tab: 
 Export From = Display Part 
 c. Browse and set the option 'Settings File Load From' to the 
 igesexport_wireframe.def file created above. 
 d. On the 'Data to Export' tab: 
 Export = Entire Part (This is a mandatory setting.) 
 Curves = ON 
 Surfaces = OFF 
 Solids = OFF 
 c. OK the Export to IGES Options dialog.


The IGES file created will have all edges of the model as curves.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V7.5.5
Function: IGES

Ref: 002-7004520

KB Article ID# PL7004520

Contents

SummaryDetails

Associated Components