---------------
Seeing "UNSUPPORTED" features being reported in the debug.log file. How can
you get rid of them.
Solution
If you are using an environment variable "SEDEMON_LICENSE_FILE" or the
"USE_SERVER" option in your license file, then you will see warning messages
similar to the following in your debug.log file:
UNSUPPORTED: "SOLIDEDGEACADEMICU" (PORT_AT_HOST_PLUS )
Administrator@edgese (License server does not support this
feature (-18,327))
This is only a message and has no impact on your ability to check out a
license. If however you feel the need to get rid of these messages, you can do
so by editing the "sedemon.opt" file that is found on the license server in the
C:/seflex/program folder. Edit this file using notepad and enter the following:
NOLOG UNSUPPORTED
This will turn off the reporting of the unsuported message in the debug.log
file.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: SETUP
Function: LICENSING
Ref: 002-7002603