Capped via definition in Valor NPI

2024-07-16T09:11:02.000-0400

Summary


Details

  • How does Valor NPI determine if a via is capped?
  • What attributes does Valor NPI use to "decide" if a via is capped when performing Assembly and Fabrication analysis?
  • Where can I read about capped vias in the Valor NPI documentation?

==================================================

 

Capped vias are defined in Valor NPI documentation in several places.

The most complete definition of capped vias can be found in Valor NPI Assembly Analysis User Guide, under Padstack Analysis.   

Valor NPI Assembly Analysis User Guide (siemens.com)

“Vias can be capped or uncapped, as determined by the boolean attribute

Capped Via. If the outer layer pad if a via has this attribute, the via is

considered capped on that side of the board. When referring to the drill

layer feature of the via, the via is considered capped when either of its

outer layer pads has the Capped Via attribute..”

Also, most analysis categories that report capped vias in various contexts include a definition of capped.

In Valor NPI Fabrication Analysis User Guide, you will note that there is a control put on this definition (for fab analysis) by the erf variable v_exposure_by_is_capped:

Valor NPI Fabrication Analysis User Guide (siemens.com)

v_exposure_by_is_capped -  Controls how a via is considered exposed.

no — A via is considered exposed if not covered in

the solder mask layer. (default)

yes — A via is considered covered if assigned

attribute Capped Via, even if exposed in the solder

mask layer.

If you are using MRA-R for Fabrication Analysis, this modifier can be found in the ACM under the name “Signal – Report capped vias

If Valor NPI System Management User Guide, you will also find the following definition (using the internal attribute name .is_capped):

Valor NPI System Management User Guide (siemens.com)

 

KB Article ID# MG604258

Contents

SummaryDetails

Associated Components