Running Valor NPI as a stand-alone server. Running Valor NPI in Database mode. After logging into a VPN, Valor NPI will not start, giving the error message "gen_com-5009-Socket connect problem".
Logging onto a VPN can change the computer's IP address, which will cause the GND (ran by the Valor GND Server) to be unreachable.
If fail to restart the Valor GND Server, please add the application program %VALOR_EDIR%\gnd\gnd.exe under Control Panel\All Control Panel Items\Windows Defender Firewall\Allowed apps.
If there still is the same error when invoke Valor NPI, please uninstall the GND service using the script uninstallGND.bat and reinstall the GND service using the script installGND.bat in C:\MentorGraphics\Valor\vNPI_2311\edir\misc.