This article serves as a guide for setting up a copy of a Capital database to test the migration steps to a new version of Capital. The steps to create the test Oracle database should be performed by a qualified database administrator (DBA). After creating the database copy, the steps to upgrade are to be followed strictly from the upgrade guide document.
To test the upgrade steps before migrating to a new version of Capital, an equivalent test/development environment must be set up with the same Oracle version and Capital version used in production.
Steps for DBA to create a copy of the Capital Oracle database for the migration test:
Once the database has been copied, install the same Capital version as in production, following the "Install Guide for Capital on Oracle" using the new test environment Oracle Connection Details. Caution: Do NOT select to Configure database for the first time as the database already exists.
Now you have a replica of the production environment and can proceed to follow the "Upgrade Guide for Capital on Oracle" for the new version.