When running Xpedition DFM, no DFM Profiles (Classification Sets) show up in the plugin.
When Xpedition DFM starts up, the DFM Profile pulldown is empty:
If the Xpedition log is viewed, there may be a message such as this:
01/24/25 06:45:25 ***Error***: The process failed : C:\MentorGraphics\Valor\vNPI_2409\edir\misc\rcom.exe -a11001 "COM get_stage_names, output = C:\Users\AppData\Local\Temp\6271.tmp", error = 1
01/24/25 06:45:25 ***Error***: No stages available
This indicates that the RCOM process, which accesses Port 11001, has failed. This process is used to get the Stage Names and other data.
Check the Port access (using a program such as "netstat") to make sure that the Port is available for the application.