OPCENTER X 2501 ON CLOUD - WHAT'S NEW
Functionalities Enhanced / Added in 2501
Order Management
- CNC Machinery now allows you to edit and delete CNC files
- Create Process Definitions without specifying the Final Material
Data Acquisition
- Selective rollback in Work Order details
- Validation on rollback of produced Material
- Usage tracking task
- Rework flow task in Operator Terminal, support to rework flows
- Rollback of consumed material
Interoperability
- Http Connector Management user interface
- New Kafka Connector supporting the publishing and consuming of Kafka messages
- OPC UA Connector supports subscription to data changes
- OPC UA Connector supports subscription to events
- OPC UA Connector supports browsing of OPC UA nodes
- OPC UA Connector supports fetching of OPC UA historical data
- Improved organization of Interop model
- New troubleshooting documentation for Interoperability
- Two new columns have been added to the Detailed View: Open NC and Closed NC, which show the count of open and closed Non-Conformances for the work order
- The new Active Non-Conformance tile has been added to the Summary View. It shows the number of open work orders that currently have at least one open non-conformance
- You can now click
on one of the tiles of the Summary View to filter work orders in the Detailed View by the total shown on that tile
Non-Conformance Management
- Implemented additional new fields: "Description" and "Responsible User" in General tab, available during creation process
- Show additional columns: "Created by" and "Responsible User" in the Overview page
- Sending Non-Conformance Data via NATS message – Updated with additional properties in the message
- Failure Pattern Search updates
- Show Attachment icon indicator
- Show Classifications icon indicator
- Select a failure with a single click and view its children by clicking on the icon
- Taking live pictures for attachment component
- Rework Handling with T&T: Operator is able to decide the Rework Work order-operation, where the rework should be carried out
- Option is available in the General tab of Non-Conformance creation
- Fetching of Work Order Operation for MTU in General tab is extended
- Updated Action description as Label controlUX enhancements and validation of Serial number in General tab
SPC Inspection and Evaluation
- Import button for gages in Gage App
- Export Management Results from Opcenter X Quality
- Graphical defect location acquisition for visual characteristics
- Check process and creation from Non-Conformances for attributive/visual characteristics
- MVP Control Chart with eCharts
- Support gage groups as filter for gages in Acquisition
Process Designer / Inspection Planning
-
- Assign Gage Group to an inspection step
- Support rework process integrated with MES
- Image support on visual inspection
- Design Rework flow
Opcenter X Configurator
Assembly of Resources
It is now possible to assemble multiple Resources to a Resource. This helps to create a hierarchy of Resources. Likewise, it is also possible to disassemble the Resources.
Defining State Machines
It is now possible to define a State Machine for the state tracking of a Resource.
You start by creating a State Machine, define various Statuses on the State Machine, and configure transitions on the states. The Resource Class gets a new Attribute - Status to enable you to associate the State Machine. Resource created from such approved Resource Class, holds the State Machine details.
For more information, see the OPCENTER X 2501 Release Notes, available in Support Center.