HyperLynx Workshops are now hosted on Xcelerator Academy (XA), the cloud-based training platform Siemens uses to deliver product training 24/7. You can learn HyperLynx workflows on-demand, without having HyperLynx installed on your local machine or tying up one of your company’s existing HyperLynx licenses.
With Xcelerator Academy, you register for a training library that contains one or more workshops (or courses), that are called learning paths. HyperLynx Workshops are delivered as part of a free library – the library has a nominal cost, but a promotional code is provided to bring the cost down to $0.
The HyperLynx Workshop library provides access to all the HyperLynx Workshops in a single place. To register for this library:
• Confirm the $0 cost and select “Proceed to Checkout”
• Fill-in your contact information and select “Continue”
• Agree to the Xcelerator Academy use terms and select “Continue”
• Reconfirm the $0 cost and select “Place Order”
• Select “Redeem Product”
• Agree to the terms and conditions, then select “Complete Redemption”
• Use the following link to access the Modern UX workshops: Modern UX Workshops
• [Serial Links] Post-layout PCIe Gen3 Compliance Verification
• [Serial Links] Compliance-based serial link and verification
• [DDR] DDR5 model-free post-layout verification
• [DDR] DDR4 power-aware analysis
• [Power Integrity] DC Drop analysis
• [DRC] Design Rule Checking – DDR4-based rules
• [Analog Simulation] AMS parasitic extraction
• Use the following link to access the Classic UI workshops: Classic UI Workshops
• [Serial Links] Post-layout PCIe Gen3 Compliance Verification
• [DDR] DDR5 model-free post-layout verification
• [DDR] DDR4 power-aware analysis
• [Power Integrity] DC Drop analysis
• [Power Integrity] HyperLynx decoupling with AMD Versal devices
• [DRC] Design Rule Checking – DDR4-based rules
• [DSE] Optimizing a differential via
You run HyperLynx on Xcelerator Academy by accessing a remote Windows desktop in the cloud, using a HTML5-enabled browser.
• The first time you run a Virtual Lab, the startup process can take up to 20 minutes. Subsequent invocations will be faster.
• Instructions for running the virtual lab should be downloaded from the same page you use to start the virtual lab:
• You access the VM desktop using a HTML5-enabled browser (we recommend Chrome). The access page lists the Citrix client first, but we recommend using HTML5 instead:
If, at some point in the process you see a message asking you to download the Citrix receiver, click on “Got It!” to skip the download, since you’re not going to use it anyway.
After learning simulation workflows with HyperLynx Workshops, you can use Xcelerator Academy’s extensive set of HyperLynx training libraries to expand your simulation skills:
• HyperLynx DRC
• HyperLynx DRC Rule Writing
• Practical HyperLynx Methodology
• HyperLynx Power Integrity Analysis
• HyperLynx Signal Integrity Analysis
• HyperLynx DDR Interface Analysis
• HyperLynx DDR5 Interface Analysis
• HyperLynx Serial Channel Design
• HyperLynx Advanced Solvers
Xcelerator Academy HyperLynx On-Demand Training