Process Preparation / Process Preparation X Machine packages not updated automatically after the installation of 2410

2024-12-10T14:15:02.000-0500
Process Preparation X

Summary

Machine packages were not updated automatically in the end of the installation


Details

When running the 2410 installer, machine package update should run automatically in the end of the installation process. In certain systems this does not happen. Reason for this is currently unknown. If you notice that machine packages were not upgraded in the end of the installation process, update the packages manually. Instructions available here:

Machine model update

KB Article ID# KB000156050_EN_US

Contents

SummaryDetails

Associated Components

Assembly Line