Upon attempting to sign an annex, if the annex is signed more than three times with an incorrect user account (one without the necessary permissions), the following message will be displayed, and the annex will be blocked
Issue Description
When attempting to sign an annex, if the annex is signed more than three times using an incorrect user account (one without the necessary permissions), the system will display an error message and subsequently block the annex.
Error Message
After several unsuccessful attempts, the following error message may be displayed:
Once this error message appears, the annex will be locked, preventing further signing attempts.
Cause
This issue occurs because the system is designed to prevent unauthorized access and modifications. When an incorrect user account is used repeatedly, the system locks the annex to protect the integrity of the data.
Workaround
To resolve this issue, you can use the following workaround:
Once the lock is removed, you can attempt to sign the annex again using the correct user account with the necessary permissions.
This can be done using the UserPro module. Assign the necessary rights to all relevant users to enable them to use the pharma modules effectively.
Steps to Assign Permissions
By following these steps and best practices, you can minimize the occurrence of this issue and ensure smooth operation within your system.
Below are other useful knowledge base articles you can find related to the same topic:
Impossible to add annex in PI process using a shared folder
Annex viewer can't display files.