Channel Adapter Adapter_Name specified in the Outbound Message Name_id does not exist

2024-11-26T14:23:56.000-0500

Summary

Messages are not processed correctly in CN-MOM


Details

In a HA CN-MOM architecture with 2 CN-MOM nodes, messages are not correctly processed from a specific adapter

the error is 

Exception in SendMessageToEachAdapter. Error Message: Error: Channel Adapter miotestadapter_test_clearcontents specified in the Outbound Message Testcommandoemoutbound_mioclient3128618 20_8ae4189d-02c6-4fb6-a8d4-aa9baa8486b1 does not exist

 

the miotestadapter_test_clearcontents  is existing, but the miochannelsource_test is a channel source not present and related to an old configuration

 

The solution is to change in the right part of the screen the right channel source

KB Article ID# KB000155449_EN_US

Contents

SummaryDetails

Associated Components