How to install Siemens License Server and configure user machines to run Simcenter Amesim 2410?

2024-10-28T17:19:49.000-0400

Summary

This article describes how to install the Siemens License Server based on FlexNet Publisher (FNP) and configure user machines to run Simcenter Amesim 2410. It requires to have already received a compatible license file.


Details

Install the license server

Siemens License Server based on FlexNet Publisher (FNP) needs to be installed on the server machine. Please download the last version of the tool from Support Center.

Select the appropriate file according to the server's OS:

Run the installer on the server machine and provide the new license file during the installation. In case you need to handle several license files, you can run this installer again, select add/replace a license file and add new licenses to the pool. It is important to keep the installer as any changes you want to make to the server will be made by running this installer again.

In case you need help or need more information about the installation, please refer to the official documentation: Siemens Digital Industries Software License Server Installation Instructions and Getting Started with Siemens Advanced Licensing Technology (SALT) and the Siemens License Server (SLS)

 

Configure the user environment

To ensure the connection between the user machines and the server, two environment variables are needed on the user machines:

    • SC1D_LICENSING_TYPE=ugs
    • SPLM_LICENSE_SERVER=29000@server_name

Reminder: Siemens License Server (FNP) will use ports 29000 and 29001 by default. Do not forget to adapt the firewall settings to open these ports on the server machine and then to ensure the users can reach both.

Always run the installer in case you want to apply modifications to the server like adding/replacing a license file, changing the ports, etc.

KB Article ID# KB000155004_EN_US

Contents

SummaryDetails

Associated Components