How to check connections in thermal coupling?

2024-09-29T04:19:59.000-0400

Summary

This article shows how to visualize thermal connections before and after solving the model.


Details

Visualizing thermal connections before solving the model

You can display connections between primary and secondary elements before solving the model only in the Thermal Coupling simulation object of type Thermal Coupling with projective intersection coupling method by selecting the Show Ancillary Display check box.

 

A diagram of a buildingDescription automatically generated with medium confidence

 

A screenshot of a computerDescription automatically generated

The ancillary display supports thermal couplings of 0D, 1D, and 2D elements, edges of 2D elements, and faces of 3D elements when they can infer an area for each type.

Visualizing thermal connections after solving the model

You can request and display the Thermal Connections and Coupled Area Ratio result sets for solved solutions with one or more following supported boundary conditions:

Table 1. Supported boundary conditions

Simulation object

Type

Solver environment

Thermal Coupling

Thermal Coupling, Perfect Contact

Simcenter 3D Thermal/Flow, Simcenter 3D Electronic Systems Cooling, Simcenter 3D Space Systems Thermal, Simcenter 3D Multiphysics

Thermal Coupling - Convection

Convection Coupling, Duct Node Convection Coupling

Simcenter 3D Thermal/Flow, Simcenter 3D Electronic Systems Cooling, Simcenter 3D Space Systems Thermal, Simcenter 3D Multiphysics

Edge-to-Edge Contact

Manual

Simcenter 3D Multiphysics

Edge-to-Edge Gluing

Manual

Simcenter 3D Multiphysics

Surface-to-Surface Contact

Manual

Simcenter 3D Multiphysics

Surface-to-Surface Gluing

Manual

Simcenter 3D Multiphysics

In Simcenter 3D Multiphysics, request Thermal Connections and Coupled Area Ratio by right-clicking the solution and selecting Edit. On the Results Options page, edit the Thermal Output Request.

 

A screenshot of a computerDescription automatically generated

In Simcenter 3D Thermal/FlowSimcenter 3D Space Systems ThermalSimcenter 3D Electronic Systems Cooling, right-click the solution and select Edit. On the Results Options page, under the Thermal tab, select the Thermal Connections and Coupled Area Ratio check boxes.

Use Thermal Connections — Elemental to display the lines representing heat paths created by the thermal solver between primary and secondary elements of supported thermal couplings. Each color represents one thermal coupling. The colors are assigned randomly and cycle through 16 predefined colors. The numbers in the legend are only indicators and do not represent the coupling magnitude.

In the following example, the thermal connections are presented for the tire (1), brake pad (2), wheel (3), and axle (4). The blue color shows the connection between the wheel and the tire, the green color shows the connection between the wheel and the brake pad, the red color shows the connection between the axle and the wheel. In the second image, note the incorrect additional connections between the wheel and the break pad, as a result of improper thermal coupling set up. After adjusting the thermal couplings, the third image accurately presents the expected thermal connections.

 

A diagram of a circular objectDescription automatically generated

 

A green and blue wire mesh on a white plateDescription automatically generated

 

A drawing of a circle with a numberDescription automatically generated

Break model

Wrong thermal connections

Correct thermal connection

Use Coupled Area Ratio — Elemental to display the ratio of the primary element area that overlaps with secondary element selection over the primary element area. This value can be higher than one when the primary elements are used in more than one supported thermal coupling.

In the first image, note that the ratio in the brake pad to wheel connection is significantly less than 1 in some areas, indicating that the thermal coupling is incorrectly defined. In the second image, the coupled ratio is equal to 1, signifying that the thermal connections are correctly established.

 

A model of a circular objectDescription automatically generated

 

A wireframe of a circular objectDescription automatically generated

Wrong thermal connections

Correct thermal connections

For a transient analysis, these result sets are displayed under the Time Invariant node in the Post Processing Navigator.

Inspecting coupling areas per element in scratch files

You can inspect elemental coupling areas in the solver, by converting the MODLCF file to ASCII format either by:

  • Using the executive menu command.
  • Specifying a FILES MODLCF, VUFF, MODLF IN ASCII advanced parameter.

 

A screenshot of a computerDescription automatically generated

 

From the MODLCF file below, we can see the surface element 66974 is connected to element 67375 and 67376.

A computer screen with a red lineDescription automatically generated

 

Displaying thermal connections per boundary condition

You can display thermal connections individually for each supported boundary condition listed in the Supported boundary conditions table.

In the Simcenter 3D Multiphysics environment, right-click the solution and select Edit. On the Results Options page, edit the Thermal Output Request and select the Create Groups for Boundary Conditions check box.

 

A screenshot of a computerDescription automatically generated



In the Simcenter 3D Thermal/FlowSimcenter 3D Space Systems Thermal, and Simcenter 3D Electronic Systems Control environments, right-click the solution and select Edit. On the Results Options page, select the Create Groups for Boundary Conditions check box.

 

A screenshot of a computerDescription automatically generated



In the Post Processing Navigator, these results are stored in the Groups node under the post view node.

 

A computer screen shot of a computer programDescription automatically generated

 

KB Article ID# KB000153742_EN_US

Contents

SummaryDetails

Associated Components