How to Inherit Polygon Attributes from an Assembly CAD into the Idealized Part (iprt) and FEM/SIM Files

2024-10-07T14:47:03.000-0400

Summary


Details


This video demonstrates the correct approach/workflow to be able to inherit attributes given at the assembly CAD level into the idealized part, fem and sim files. Many users create CAD assemblies and give attributes to their components at the assembly level, then they try to see these attributes reflected in the idealized part and fem/sim files without success. This approach is wrong as attributes given at the assembly level are not inherited by iprt and fem/sim files. In order to see attributes reflected in iprt and fem/sim files, these must be given at the root component level, that is, at the individual part/component alone, rather than when it is already assembled.

KB Article ID# KB000153650_EN_US

Contents

SummaryDetails

Associated Components