Simcenter Nastran license error: No such feature exists. (-5,346)

2024-09-26T16:50:30.000-0400

Summary

How to troubleshoot the Nastran license error "No such feature exists. (-5,346)"?


Details

User gets the following error during a rerun of an old simulation after switching from legacy licenses to license bundles. It lists several license features missing with the same error code as shown below. 

 

8:49:10 (ugslmd) UNSUPPORTED: "SC12500_ug_nas_bn" (PORT_AT_HOST_PLUS   ) abc@XYZ  (No such feature exists. (-5,346))

8:49:10 (ugslmd) UNSUPPORTED: "NX93300_ug_nas_bn" (PORT_AT_HOST_PLUS   ) abc@XYZ  (No such feature exists. (-5,346))

8:49:10 (ugslmd) UNSUPPORTED: "ug_nas_bn" (PORT_AT_HOST_PLUS   ) abc@XYZ  (No such feature exists. (-5,346))

8:49:12 (ugslmd) UNSUPPORTED: "nx_nas_basic_dsk" (PORT_AT_HOST_PLUS   ) abc@XYZ  (No such feature exists. (-5,346))

 

This is due the changes in configurations between legacy and bundle licenses. Switching the License Type from the default Desktop to Enterprise in Solver Parameters (RMB on active solution -> Edit Solver Parameters) before solving will resolve this license error. 

KB Article ID# KB000153648_EN_US

Contents

SummaryDetails

Associated Components