Process Preparation / Process Preparation X Tip how to avoid overwrite shapes when transferring program to SiplacePro.

2024-09-19T07:03:05.000-0400
Manufacturing Systems Solutions Data Preparation Import and Export Data Analysis Auto-Assembly Station Configuration Assembly and Documentation Test Engineering Test ViewStation Libraries

Summary

When transferring the board to SiplacePro, there are an update of parameters (cameras, nozzles, models, polarity - non-polarized) for all these already established and used ASM SHAPE systems. This change occurred despite the selected option to not overwrite data in the library. How to avoid Shape ,etc. overwrite by using . \\SYSTEM folder location ?


Details

Detailed explanation in the attach

Also please note following :

Good practice is to set default values in machine configuration and adjust properties in Auto -Assembly session instead. 

Notice as well that session settings  are always overwriting configuration settings.

Do desired changes on session and verify output to Siplace Pro.

 

KB Article ID# KB000153397_EN_US

Contents

SummaryDetails

Associated Components

Valor Process Preparation