Spikes in residuals and/or monitor plots when resuming simulation

2024-09-13T20:07:13.000-0400

Summary

Jumps in residuals and/or monitor plots are noticed when resuming a solved simulation to continue the solve


Details

When a solution is resumed from a solved case, a jump in values of the residuals and/or monitor point plots are noticed before the values stabilize again(refer image below). This is noticed especially in Joule Heating and Conduction only simulations.

Image_2024-08-21_15-10-20.png 
One of the main reasons for this behavior is that the results fields are always written as single precision (even when the double precision solver is used). Rounding errors can occur when the solve is continued and this can occasionally cause a noticeable jump in residuals. But, the accuracy of the converged results is not compromised.

KB Article ID# KB000153250_EN_US

Contents

SummaryDetails

Associated Components