Simcenter 3D Solutions Resolving Warning 4903 - Simcenter 3D Thermal

2024-08-19T04:36:33.000-0400
Samcef Desktop Samcef Wind Turbines Simcenter Nastran Simcenter Samcef Simcenter 3D Simcenter 3D Solutions Marketing TEA Pipe Simcenter ZONA BOSS Quattro Simcenter Multimech Teamcenter Share CAESAM Simcenter FLOEFD SC

Summary

This article addresses Warning 4903, a common issue encountered by users. The articles explore what this warning means, why it occurs, and provide practical steps to address it.


Details

The Warning 4903 indicates that the value is outside of the defined table.

For example, you defined the following table:

If the calculated temperature is 50 C, the solver will consider the thermal conductivity of 110 W/mK, if the temperature is 300 C, the solver will consider the thermal conductivity of 150 W/mK.

If the warning persists till the end of the solve:

  • Locate the table by its number in the INPF file, for example “ 6 ” (with spaces, without the apostrophes).
  • Review which boundary conditions or material properties might have issues.
  • Correct the table.

KB Article ID# KB000134579_EN_US

Contents

SummaryDetails

Associated Components

Samcef Desktop