How to export or import the stylesets (SystemData) from Capital Essentials?

2024-08-19T17:28:50.000-0400

Summary

This article describes how to export and how to import the SystemData.xml file.


Details

The display or graphical representation of objects in Capital Essentials is controlled via a style set. The Harness and Wiring diagram stylesets are unique per installation. To share the stylesets with another installation or with Siemens customer support, the Capital Essentials system data must be exported. The system data can only be exported via a Windows command prompt.

Prerequisites

  • Capital Manager Essentials is running.
  • You are a user with administrator privileges
  • You have created a repository directory to which the premigration utility can export the system data. It must be accessible with full read-write access.
  • During the export process, a sub-directory named "SystemData" is created within the repository directory; this sub-directory includes the file named "SystemData.xml". For a successful import, this specific file structure should be maintained.

Procedure to export

Launch a command prompt window and run the following command:
[Installation_directory]\bin\CapitalPremigrateEssentials.exe -d -u=[system_user] -w=[system_user_password] -f=[repository_directory]

Where:
[Installation_directory] is the path to your Capital Essentials installation
[system_user] is the name of a superuser which has admin privileges
[system_user_password] is the password for the superuser
[repository_directory] is the path to the repository directory

Example:

C:\Siemens\CapitalEssentials\bin\CapitalPremigrateEssentials.exe -d -u=system -w=manager -f=C:\Siemens\repository

Procedure to import

Same as above except replace the executable program "CapitalPremigrateEssentials.exe" with the import executable "CapitalMigrateEssentials.exe" in the command line.

Example:

C:\Siemens\CapitalEssentials\bin\CapitalMigrateEssentials.exe -d -u=system -w=manager -f=C:\Siemens\repository

Where:
There exists a file with the path: C:\Siemens\repository\SystemData\SystemData.xml

 

 

KB Article ID# KB000134484_EN_US

Contents

SummaryDetails

Associated Components