Opcenter Intra Plant Logistics "Scanner is not ready" message displays after launching the "Split and Splice" application.

2024-08-07T13:50:39.000+0900
Opcenter Intra Plant Logistics

Summary

The "Scanner is not ready" message changes to "Scanner is ready" after scanning data if the scanner is connected. Set "ScannerGetVersion" to "No" for it to always display "Scanner is ready".


Details

This is by design, and the message changes to "Scanner is ready" after you scan any data if the scanner is connected and configured correctly.
not ready 

ready

If you configure the "ScannerGetVersion" parameter of this "Split and Splice" resource to "No", the message will always display as "Scanner is ready".

Above behavior is confirmed base at IPL2310.

KB Article ID# KB000134222_EN_US

Contents

SummaryDetails

Associated Components

OC IPL Configuration