To automatically include/update these objects from a sandbox into a Production Library, use the Additional Files tab in a Production Library object within EDM Library Cockpit.
For Layout, Panel and/or Drawing Templates, the Instructions provided in the Xpedition™ EDM Library EDA Library Module Guide do not include sufficient detail regarding the addition of complete folder structures. However, these entire folder structure can be added as an additional object.
Other files to consider adding may include:
- <CentralLibraryFolder>/Layout/JobPrefsDB.jpf
- <CentralLibraryFolder>/<customDBC>.dbc
To add customized files and/or templates to a Production Library Object within the EDM Library Cockpit, do the following:
- Open the Production Library in Modify mode:
- Select the Additional Files tab:
- If needed, click the New Object button in the lower left to add a new line, then click the Attach button at the right side.
Don't add a new line when updating an existing object; attaching an object will add a new version:
- Skip this step if updating existing objects:
For new objects, Click New at the top. The Create document dialog appears;
supply a new Document name. The Document name cannot contain spaces or special characters.
Then select a target folder within the Documents class:
Note: Consider creating a special Documents folder just for Additional Files, for example: Production Library Additional Files
- In the middle section of the form, click Browse to select the filesystem "Root directory" containing the customized objects:
- Navigate to the sandbox. Select the sandbox name, Click Open:
Note: For folder type objects such as Templates, Do NOT select the folder at this step.
- With the sandbox root path supplied, click Add,
then select the file:
For Folder type objects such as Templates, select the folder:
- Verify all fields, then click Ok.
- Click Ok to save and close the Production Library Object:
Run the Cache Manager to create or update a Production Library Cache on the file system:
- Select menu item: Tools > Library > EDM Library Cache Manager.
- On the EDM Library Cache Manager dialog, specify New or Update,
specify the filesystem Production Library Cache location,
if this is a new cache, select the Production Library object, otherwise it will be automatically filled in for an existing cache,
then click Ok to create/update the filesystem cache:
- Confirm the Additional Files were written into the Production Library Cache:
Search terms:
After creating or updating any of the following objects in an EDM Library Sandbox:
- Drawing
- Layout
- Panel templates
- Central Library Properties (Centlib.prp) file
How can these templates/files be automatically added to Production Library caches?
See related KB Articles:
MG621551: Xpedition EDM Librarian: Creating new Sandboxes with Custom CentLib.prp; Adding More Properties to Custom CentLib.prp
MG602602: EDM Library: Automatically adding Sheet Borders/Builtin and PCB Drawing objects to the filesystem Production Library cache