Simcenter 3D Solutions How to adjust the result legends as per cutting plane contour view in Simcenter 3D post processing

2024-07-23T06:51:34.000-0400
Samcef Desktop Samcef Wind Turbines Simcenter Nastran Simcenter Samcef Simcenter 3D Simcenter 3D Solutions Marketing TEA Pipe Simcenter ZONA BOSS Quattro Simcenter Multimech Teamcenter Share CAESAM Simcenter FLOEFD SC

Summary

During post-processing of results, when users attempt to view the result values for a cutting plane of a part, the result legends do not adjust automatically. Consequently, the color contour, which references the legend values, corresponds to the full component result rather than the displayed section achieved through the cutting plane. Simcenter 3D Post processing Result Legends Result Contours


Details

Issue:

During post-processing of results, when users attempt to view the result values for a cutting plane of a part, the result legends do not adjust automatically. 
Consequently, the color contour, which references the legend values, corresponds to the full component result rather than the displayed section achieved through the cutting plane.

Work-around:

Here it can be seen that for the cut plane, the min and max results values are different from the mentioned legends extremes.

So, the around for this is, after setting the cutting plane, toggle on MIN and MAX of annotation and set those values as min and max in the specified like below snapshot.

KB Article ID# KB000133857_EN_US

Contents

SummaryDetails

Associated Components

Samcef Desktop