How do I find the Contact Surface between two specific Parts for use in Reports and Scenes?

2024-07-23T08:12:55.000-0400

Summary

By using three successive filters with a referencing query, it is possible to find the part contact surface generated between two parts.


Details

In a Parts based workflow it is often beneficial computationally to reduce the number of regions and interfaces.  It is also often the case that the Geometry Part Surfaces are not split and named separately, so finding the object for reports or debugging contact surfaces can be difficult.

 

For example, with Block Parts with a default surface name, after an Imprint or Contact Creator operation a new class of surface called a Part Contact Surface is generated, as shown in the following image.  With the default naming convention, it is difficult to know which surface corresponds to which part.

Screenshot10.png

This article will show you how, with the use of filters, you can find the part surfaces generate by contacts between specific parts.

 

Firstly, you need to create a filter (1_PartContact) with the following predicates;

  • Type is Part Contact
  • Relationship referencing [Select first Part]
  • Relationship referencing [Select second Part]

Screenshot2.png

 

To get the Type is Part Contact you can go in the Simulation Tree to Geometry>Contacts and drag and drop one of the folders.

Screenshot6.png

 

Next create a Second Filter (2_PartSurfaceContact);

  • Type is Part Surface Contact
  • Relationship below in tree 1_PartContact

Screenshot3.png

 

Again you can drag and drop a contact in the subfolder to get this specific Type.

 

Now create a third filter (3_PartContactSurface)

  • Type is Part Contact Surface
  • Relationship referencing 2_PartSurfaceContact

 

Screenshot4.png

This surface type is not on the main simulation tree so the best way to select this is via the filter Type is Other (drop down list) and navigate to a Part Surface that has a subfolder as shown in the top image.  Note you will need to have had a Imprint or Contact Creator Operation activated.

Screenshot15.png

 

Screenshot14.png

Now you can use this third filter for the query entry for you Reports and Object Displayers.

 

Screenshot11.png

Screenshot13.png

KB Article ID# KB000133693_EN_US

Contents

SummaryDetails

Associated Components