This article covers how to download and install Simcenter Testlab 2406 software. Simcenter Testlab 2406 was released in July of 2024.
Article contents:
1. Downloading the Simcenter Testlab software
2. Installing the License Server
3. Installing the Simcenter Testlab software
3.1. Preparing Installation
3.2. Installing Prerequisites
3.3. Installing Hardware Diagnostics
3.4. Installing Simcenter Testlab
4. Download and Installation of 1D and 3D Drivers
4.1. Downloading Drivers
4.2. Installing Drivers
1. Downloading the Simcenter Testlab Software
Video: Simcenter Testlab 2406 Download
First download the software from the Siemens Support Center:
A ISO file is a single file that contains all the installation files. An ISO file is an "Image" file that can be burned to a DVD if desired. However, it is not necessary to burn it to a DVD to install it. It can be installed directly from the ISO file on a PC. See the instructions below for how to do this.
More information about ISO files can be found here: https://en.wikipedia.org/wiki/ISO_image
2. Installing the License Server
If installing Simcenter Testlab on a network with access to a central license server, it is not necessary to install the License Server on the local machine. Skip ahead to section 3.
If the license will be local to the PC, the license server software needs to be installed. See the article Simcenter Testlab: RLM License Server 15.1 Installation and Setup for more information.
3. Installing the Simcenter Testlab Software
Video: Simcenter Testlab 2406 Installation
After the software has been downloaded, the installation can start.
3.1 Preparing Installation
Using the ISO file in Windows file explorer:
To extract the installation files from the ISO file:
After extracting or mounting the files, several directories and an "autorun.exe" file should be available as shown below.
Right click on the file that says “Autorun.exe,” and select “Run as Administrator.” You need full administrator rights on your computer to install.
The main installation menu should appear. Select the top option, “Install Simcenter Testlab,” to begin the installation.
3.3 Installing Hardware Diagnostics
The pop-up window for the Simcenter Hardware Diagnostics will come up. This utility is used to scan Simcenter SCADAS hardware and make a diagnostic report.
Certain functionalities of Simcenter Testlab use the Microsoft ODBC driver; since the 2406 release is 64-bit, these features may not work if the 32-bit version of the Microsoft ODBC driver is installed. To determine how or whether to switch drivers, please refer to the article Simcenter Testlab 2306 - Resolving ODBC data source issues caused by Microsoft Access Database Engine installation.
When coming to the screen asking to fill in the license file or the license server, select the box “Use a license server.”
Questions or issues? Please contact Siemens Support Center at the appropriate phone number listed on https://support.sw.siemens.com and have your sold-to number (sold-to is in license file, or choose Help -> About Simcenter Testlab from the software interface). The phone number for North America is 1-800-955-0000.
See Simcenter Testlab: RLM License Server 15.1 Installation and Setup for information on how to install the RLM license server and set up your Testlab license file to complete the Testlab software setup.
See Which files should I download for Simcenter Testlab 2406 for more information on the files and other product components available in the download area of Simcenter Testlab 2406.
Have new Simcenter SCADAS hardware? Check out the articles What’s in the box? Getting Started with Simcenter SCADAS and Getting Started with Simcenter Testlab.
Other Simcenter Testlab Installation Resources: