Capital™ Plugin not being loaded by Capital

2024-08-19T17:29:49.000-0400
Capital Device Modeler Capital Capital Harness Process Designer Capital Harness Designer Capital E/E Reporter Capital Connectors Capital Harness Costing Capital Dictionary Capital CostingXC Capital Systems Integrator Capital Component Manager Capital Harness Designer Modular Capital Logic Designer Capital Project Manager Capital E/E Publisher Capital Symbol Designer Capital Wiring Integrator Capital Access Manager Capital Work Instruction Publisher Capital Systems Architect

Summary

Typically when a plugin jar file is placed in your Capital plugins folder, you would expect that the plugin would appear when you go to "Capital > System > Plugins" in the ribbon menu. There are some cases where plugins may fail to load due to errors in the configuration of coding of the plugin. In most cases an error will be reported in the output window if a plugin fails to load.


Details

Check your Capital log files for any plugin errors and resolve the errors.

There is one case where plugins may fail to load but no error is reported. This can occur if you name a package name in conflict with Capital's existing class paths.

For instance: The capitalapi.jar file contains a class path "com.mentor.chs.plugin.drc" where various classes are located for plugin DRCs.

If you create a plugin DRC and set the package name where the plugin is located to "com.mentor.chs.plugin.drc", the plugin will not be loaded and no error is reported.

KB Article ID# KB000133330_EN_US

Contents

SummaryDetails

Associated Components

Capital Device Modeler