Simcenter 3D Solutions Transmission Builder - Asymmetric Gears

2024-06-21T11:59:31.000-0400
Simcenter 3D

Summary

Starting with version 2406, Simcenter 3D Motion Transmission Builder allows the definition of asymmetric spur and helical gears based on different pressure angles and the left and right flanks of the gears.


Details

To define asymmetric gears, select the Asymmetric Gear option in the Gear Mesh Pair (Fig. 1-a).

Once the Asymmetric option has been selected, both the Left and Right Normal Pressure Angle parameters can be defined. (Fig. 1-b, c).

Fig. 1 Defining Asymmetric Gears in Transmission Builder

fig01_tb.png

The following figure (Fig. 2) shows such an asymmetric gear pair.

Fig. 2 Asymmetric Gears in Simcenter 3D Motion

fig02_mot.png

Note that for Asymmetric Gears on should make use of either the Analytical Empirical or Advanced FE Preprocessor calculation methods in the Gear Contact.

KB Article ID# KB000133324_EN_US

Contents

SummaryDetails

Associated Components

Motion