How to extract max result values from contours and plot as a function of frequency?
This video shows how to extract max result values from result contours available at a number of frequencies and plot them as a function of frequency in Simcenter 3D. We can use the post-processing options like "Result Variable" and "Result Probe" available in Simcenter 3D to do so. The process is demonstrated here using the acoustic pressure results from an example acoustic radiation model but the same approach can be applied to other models and results as well.