What are the locations of the Local and Global BOM Manager Parameter files?
The BOM Manager Parameters file name is: bommgr_chk_tolerances
The Local location is: %VALOR_HOME%/.genesis directory
The Global location is: %VALOR_DIR%/sys directory
The Local file is used if it exists even if the Global file also exists. This is the general practice of Valor NPI.
File contents as of Valor NPI version 2403:
# BOM Manager check avl default tolerances
BODY_X_TOL 0.1
BODY_Y_TOL 0.1
HEIGHT_TOL 0.1
PIN_SIZE_TOL 0.01
PIN_LOC_TOL 0.01
CHOSEN_BY 0
IMPORT_RECOM 0
ACCEPT_RECOM 0
PITCH_2_PIN_TOL 20
PITCH_3_PIN_TOL 10
PITCH_N_PIN_TOL 5
BODY_X_LOWER_TOL 50
BODY_X_UPPER_TOL 10
BODY_Y_LOWER_TOL 50
BODY_Y_UPPER_TOL 10
USE_BOM_IMPORT_WIZARD 1