Connect Platform NATS cluster connectivity for CN EL <-> EX EL Integration is available as field fix in the following versions: 2310.x, 2404.x
Connect Platform NATS cluster connectivity for CN EL <-> EX EL Integration is available as field fix in the following versions: 2310.x, 2404.x
NATS cluster connectivity was added to the line manager to enable connection to Connect Platform NATS cluster
In line manager properties set the
Nats Servers URLs
property to contain the NATS servers of the cluster
The format is server address1:port1;server address2:port2;...