The FLOEFD Remote Solver can be installed on Rocky and Alma Linux which are both supposed to be binary compatible but the service itself cannot be started. An error message 'ERROR: failed to determine your linux distribution' is thrown.
The reason for this unwanted behavior is the check for the name of the Linux distribution in the shell script cmn_utils.sh This script can be found in /usr/local/EFD2312_0001/bin (assuming a standard installation; otherwise use find). This shell script provides a function that checks for SuSE, Red Hat, Debian, Ubuntu and CentOS but not (yet) for the newer distributions Rocky and Alma Linux.
By editing the script can be made aware of the two distributions.