Calibre How to group & filter Calibre® PERC™ results using Calibre® PERC™ RVE

2024-04-08T11:16:06.000-0400
IC Verification & Signoff Viewing & Interfaces

Summary

his video shows how to use the bookmark feature in Calibre® PERC™ RVE to sort and filter the results based on the properties attached to the different PERC-checks and then re-use this criteria across multiple RVE sessions


Details

Users who do Calibre® PERC™ debug using Calibre® PERC™ RVE, desire different sorting and grouping criteria for different PERC-checks such as floating-gate, gates tied to supply etc.

This video shows how to use the bookmark feature in Calibre® PERC™ RVE to sort and filter the results based on the properties attached to the different PERC-checks and then re-use this criteria across multiple RVE sessions. Users can save multiple bookmarks for specific type of checks and easily switch between bookmarks based on the type of PERC-check they are trying to debug.

The Bookmark capability is also available in Calibre DRC RVE and users can use this functionality when debugging Calibre DRC results as well. 

KB Article ID# KB000131306_EN_US

Contents

SummaryDetails

Associated Components

Calibre PERC