HyperLynx Getting Started with HyperLynx DRC Design Rule Checking

2024-09-06T23:41:15.000-0400
DRC

Summary

These are the articles which discuss basic setup and usage of HyperLynx DRC


Details

Configuration of projects in HyperLynx DRC

Most of the work done in HyperLynx DRC is setting up the project, selecting rules to run, and configuring the rule parameters. The following articles give basic information about the setup and configuration of the DRC application and projects in DRC.

Getting Started With HyperLynx DRC video series

KB000134079    HyperLynx DRC: Overview
KB000134011    Setting up a Project and Verifying Data
KB000133984    Understand Rules and Object Lists, and Limiting Scope
KB000133987    Running the DRC Rules and Viewing the Violations


KB000134039    Reusing project settings in HyperLynx DRC
KB000134068    Defining Differential Pairs in HyperLynx DRC
KB000134080    PowerNets, GroundNets and ConstantNets in HyperLynx DRC
KB000134082    Desired product license selection list at HyperLynx DRC startup
MG613171    Using the Rules Library
KB000134083    Sharing Information on Reported DRC Violations

MG611370   Webinar - Expanding your Xpedition DRC Checks to be electrically aware
         Running HyperLynx DRC directly from Xpedition using Xpedition Analysis Control (XAC)

Going Further

Please take a look at the HyperLynx DRC content in the Xcelerator Academy High-Speed PCB on-demand training track.

Custom Rules

A significant and powerful feature of HyperLynx DRC is the ability to create a custom rule for your design checking. This is an advanced complex task, but here are a few items to consider.
The HyperLynx DRC documentation includes a reference manual for the Automated Object Model (AOM) objects that you can use in custom rules. Look for the document, HyperLynx™ DRC Automation Reference in your local installation or on Support Center, depending on how your documentation is accessible.
Siemens EDA provides a training course on creating custom rules.
MG613039    Script Syntax Changes for VX.2.8
KB000134085    Enabling python script language

 

KB Article ID# KB000130859_EN_US

Contents

SummaryDetails

Associated Components

HyperLynx DRC