Cause: In version 2304 some of the features added requires support for OpenGL version 2.0 or higher. Machines running lower versions of OpenGL encounter this crash.
Remedy: Update the machine to run on OpenGL version 2.0 or higher.
Workaround:
Note: This is an internal environment variable provided to allow users carry on working on the machine with minimal disruption. As it is an internal variable it is not fully tested and some aspects of the software may not work correctly.