How to access the Standard Examples of Insight Analyzer

2024-05-01T10:48:33.000-0400

Summary

This article illustrates the steps to access and run the Standard Examples of Insight Analyzer


Details

The Insight Analyzer has hundreds of mini example projects that can demonstrate a particular concept, check, violation, or setup method.

 

There are two ways to access the examples:

  1. It can be accessed directly in the examples folder in the Insight install location
  2. Through the GUI

The instructions to access these examples through the GUI are as follows:

  • In the GUI, select Help > Reference Examples

  • Use the search tool to find the examples based on a keyword, or open the PDF containing all the examples through the link

Note: there is a button "Exact" that can be clicked to narrow down the results.

For example:

  • Search for "nor isolation", and the results will appear

  • When clicking on the "Exact" button, the results will be narrowed down as shown

  • Click on the link to open that example in the large roll-up PDF 

  • To run any of the examples in the document, follow the instructions in the second page of this document

 

KB Article ID# KB000130599_EN_US

Contents

SummaryDetails

Associated Components