An example is provided based on the surface chemistry tutorial with multiple ease of use improvements.
Attachments: | surfaceChemistry_userCode.7z (1 MB) |
Reaction rates play a crucial role in understanding and predicting chemical reactions. They determine how fast a reaction occurs and are essential in various fields, such as chemistry, physics, and engineering. Simcenter STAR-CCM+ allows the import of all CHEMKIN defined reaction rates by default. In some cases this is still too limited. For these situations the user-coded Modified Internal Rates of Individual Reactions was introduced in Simcenter STAR-CCM+ 2310 allowing researchers and engineers to customize and modify reaction rates based on their requirements. With user code you can program freely in c, c++ or Fortran - even using external libraries if necessary.
For the latest information on this method please conduct the latest version of the User Guide: Home > Physics Simulation > Reacting Flow > Reacting Flow General Reference > Reacting Model Reference > User-Defined Reaction Rate Source Terms
User Coding for Reaction Rates provides a flexible approach to adjust reaction rates by accessing relevant data through a structured interface and even utilizing user-defined field functions. This method offers these main inputs:
One challenge with User Coding for Reaction Rates is the handling of indices. The indices of species, reactions, and field functions can change as new elements are added or removed. To address this issue, a workaround involves defining an enum to assign names to species, reactions, and field functions. This approach enables the use of names instead of indices, making the code more readable and maintainable.
For example: here, we adjust the (forward) reaction rate of "CH4+2PT(S)=>CH3(S)+H(S)" by using the partial pressure of CH4, with the forward reaction rate reacRateForward and the partial pressure of Methane pi[CH4].
reacRateForward[_CH42PTStoCH3SHS] *= 1 / (1 + pi[CH4]);
Next example: here, we modify the reaction rate of all reactions based on a user field function f[_onOff]. For testing purposes, the user function dynamically deactivates certain cells by multiplying by either 0 or 1. The User Field Function $_onOff and the resulting Chemistry Heat Release Rate is shown in the first two animations of the example surface chemistry simulation.
for (unsigned int i = 0; i < nReactions; ++i) {
reacRateForward[i] *= f[_onOff];
reacRateBackward[i] *= f[_onOff];
}
The enum indices can be either read manually from the interface or created using user code. Simply define the VERBOSE output option in the code and run once. This creates the indices automatically in the output, copy paste them into the enum definition on top.
typedef enum {
CH4, CO, CO2, H2, H2O, N2, O2, OH, // fluid phase species,
CS, CHS, CH2SS, CH3S, COS, CO2S, HS, H2OS, OS, OHS, PtS, // surface site species,
PtB // bulk species IN CORRECT ORDER
} SpeciesOrder;
Another challenge with the reaction rate user coding is the limited options for debugging output. Be cautious with printf. The user code is executed for each CVODE iteration (plus numerical linearization executions) and for each cell. Therefore, each line of the user code is executed VERY often and the output using printf is massive.
A workaround is build into the provided example. You can now export field functions from the reaction rate User Coding.
This is done via global vectors storing the data during the reaction rate calculations. The stored function is recalled by a normal User-Coded Field Function and can be displayed as such. Have a look at the bottom two animations above. Here the previously used expression 1/(1+pi[CH4]) is plotted once using a User Field function '_1/(1+pi)' and the User-Coded Field Function 'User transferData' for comparison with the same result.
Be aware this method works best in serial simulations. For parallel simulations the used 'Cell Index' function is not uniquely defined.
To enable this feature please define the ENABLE_DATA_TRANSFER in the provided user code. In the line 'transferData[index] =' you can define what data you want to be transferred and shown in 'User transferData' for debugging.