The error message floview.exe pops up when trying to start Simcenter Flotherm 2310

2024-02-21T14:24:05.000-0500

Summary

I have recently installed Flotherm 2310 on windows 10 machine. When I go to launch the software, I get an error message saying floview.exe has stopped working and windows closes the program. I've tried uninstalling 2310 and reinstalling it with no luck. I have version 2210 on that machine and it works fine.


Details

Starting with Simcenter Flotherm 2304 and 2310, the Graphics Card must support OpenGL 2.0 or higher. This is mentioned in the Release Highlights of Simcenter Flotherm 2304 and 2310:
image.png
Please make sure the graphics card satisfy this requirement.

Also please make sure the Operating System of you computer is compatible with the following:

image.png
 

KB Article ID# KB000129814_EN_US

Contents

SummaryDetails

Associated Components