The von Mises stress can be enriched by a sign in order to know if we are dealing with traction or compression. This tutorial show you the workflow.
Stress Signed = σvM* sign*(σPMax)
List of features to use :
A 150 mm beam and section 10x10 mm² where a flexion is applied.
Create variables for Max Principal Stress and von Mises Stress with the feature “Result Variable”.
See below the list of variables:
The result probe creation where we define the formula using the 2 variables created just before.