Calibre Calibre: SPICE Netlist Consolidation 01

2024-10-31T15:20:48.000-0400
IC Verification & Signoff

Summary

Calibre users are under constant pressure to improve productivity. Therefore, Calibre engineers are forever looking for areas where performance is at risk. One such area involves the Source SPICE netlists and how they are constructed and stored. This video will describe this issue, how to determine if it is occurring during your Calibre nmLVS run, and how to rectify this problem.


Details

Source SPICE netlists are often built hierarchically and concatenated from multiple sources and at multiple levels.  Each level (IP, Block, Macro) may consist of multiple files spread across the network.  When this occurs, it can also possess multiple duplicate inclusions to the lower-level libraries.  How does this affect your runtime performance?  This video provides insight into this issue

 

KB Article ID# KB000129680_EN_US

Contents

SummaryDetails

Associated Components

Calibre E2LVS/V2LVS Calibre nmLVS