Simcenter 3D Solutions
Tutorial - Read contour plot with another CSYS stored in result file
2024-02-09T15:16:55.000-0500
Simcenter NastranSimcenter SamcefSimcenter 3D
Summary
User can use the Post Processing environment to adapt contour plot to a CSYS stored in the result file.
Details
By default, Simcenter 3D will open results file using the Global cartesian CSYS. But you can change it from the Post Processing. This workflow is possible only if you solve your solution with the CSYS. If you forget to create the CSYS before solving, another workflow exists.
Steps:
Create a CSYS in the sim file. Solve your Solution Load the result from the Post-Processing environment. Load the Displacement X then click on "Edit Post View" From Result tab, choose Select from the Post Processing Navigator in the after unrolling "Contour Plots" container, the Cylindrical CSYS you want to use. You have to show the CSYS before selecting the CSYS from the display area.