A plmxml file created from NX was bridged into Capital Harness Designer using Change Manager, the bundles are missing from the design.
Details
This can happen if the user doesn't have the correct File of Type selected. After clicking on Incoming, the Import Harness File dialog is displayed. The user will need to check the Files of type drop down menu and change it from NX - Wiring Integration to NX - Harness Integration.
The dialog currently set to NX - Wiring Integration:
The dialog should be set to NX - Harness Integration:
Now when the plmxml file is bridged in the bundles will be included.