1) The error message in the Log is:
*********** ERROR INTERNAL 07Dec2023.151302.078 valornpi 8232 2305.1(23029404) Windows 11
(((top_name)?(int)strlen(top_name):0) > 0) at D:\anthill3\var\jobs\projects\386472_4686998\s_dev\code\iol\iol_eda.c 3019
*********** ERROR 07Dec2023.151302.079 valornpi 8232 2305.1(23029404) Windows 11
error while reading EDA file(path - <Job Path>/
steps/pcb/layers/comp_+_top/components, line - 1736)
Status raised : module - D:\anthill3\var\jobs\projects\386472_4686998\s_dev\code\iol\iol_eda.c, line - 1622
Status raised : module - D:\anthill3\var\jobs\projects\386472_4686998\s_dev\code\iol\iol_eda.c, line - 1299
Status raised : module - D:\anthill3\var\jobs\projects\386472_4686998\s_dev\code\iol\iol_genesis.c, line - 12485
Status raised : module - D:\anthill3\var\jobs\projects\386472_4686998\s_dev\code\iol\iol_genesis.c, line - 12313
Status raised : module - D:\anthill3\var\jobs\projects\386472_4686998\s_dev\code\iol\iol_genesis.c, line - 12069
*********** ERROR 07Dec2023.151302.080 valornpi 8232 2305.1(23029404) Windows 11
unable to read layer - comp_+_top2) This indicates an error in the '
components' file at
line 1736.
3) The problem is that the '
toeprint_name' (per the ODB++ Spec) is not present at the
end of line 1736.
4) Below is a snapshot of the specific area in the '
components' file:
![image.png](media/0EMKZ000000LAxM)
5) There should be
9 fields in line
1736 but there are
only 8.
6) Compare to
lines 1737 and 1738, which have
9 fields each.
7) If the data was exported from a non-Siemens software, then the customer should be advised to take the issue up with that software vendor.