Simcenter MAGNET Suite
Modifying a full stator DXF drawing for Motorsolve's DXF import
2023-12-01T13:54:00.000-0500
MAGNET
Summary
This video shows how to modify a full stator DXF drawing into a segment for Motorsolve's DXF Import. There is no sound.
Details
This video shows how one should modify a full 360 degree DXF drawing of a stator into a half tooth + half slot segment so that Simcenter Motorsolve will accept it when using DXF import. Note that besides Simcenter MAGNET, any 2D CAD program that can read 2D DXF files could be used to modify the DXF file.