Losses in electrical machines play an important role in limiting their efficiency. The iron losses in the magnetic parts of the machine are also known as core losses or magnetic losses. They are caused by the changing magnetic field in the cores of the stator or rotor machine. The iron loss models in Simcenter STAR-CCM+ are based on the Steinmetz equation. In addition to the various extensions of the Steinmetz equation, there is another type of iron loss equation that divides the iron losses into different physically based parts. This type of model includes the Bertotti loss model, which introduces an additional loss term to take into account the excess losses as a function of flux density and frequency.
Attachments: | WoundFieldExample_BertottiLoss.sim (53 MB) |
Losses in electrical machines play a major role in limiting their efficiency. In general, the losses in electrical machines can be separated into mechanical losses, winding losses, and iron losses [1].
Workflows and examples for analysis of lots of aspects of electric machines can be found here:
The iron losses in the magnetic parts of the machine are also referred to as core losses or magnetic losses. They are caused by the changing magnetic field in the stator or rotor core of the machine. In the case of conductive ferromagnetic materials, the iron losses are often divided into hysteresis losses and eddy current losses. The former describe the losses that are attributable to the hysteresis properties of the magnetic material. If a magnetic material is first slowly magnetised with an increasing magnetic field H and then demagnetised with an opposing magnetic field, the magnetisation curve does not describe the same path back. Instead, a hysteresis curve is created. The area enclosed by this hysteresis curve is equal to the specific energy (Ws/m3) for each cycle and is therefore proportional to the iron losses [1].
Eddy currents are created by the induced voltages in the conducting magnetic materials due to the changing magnetic flux, leading to dynamic iron losses. These eddy currents counteract the variations (time and direction) of the magnetic fields. They lead to a broadening of the hysteresis curve and thus increase the magnetic coercivity Hc [1].
In addition to the various extensions of the Steinmetz equation, another type of iron loss equations divides the iron losses into different physically based parts, it is called the Bertotti Loss model. Another additional loss term pexc to account for the excessive losses as a function of flux density and frequency is introduced [1]. It divides the iron loss formula pFe into three terms: the static hysteresis losses physt, the dynamic eddy current losses pec and the excess losses pexc:
Bertotti developed a theory that led to a statistical model for calculating the iron losses by introducing so-called magnetic objects, which led to a physical description and function of the loss factor Cexc in relation to the active magnetic objects and the domain wall motion.
S is the cross-sectional area of the laminating sample, G≈0.136 is a dimensionless coefficient of eddy current damping and σ is the electrical conductivity of the laminating sheets. V0 characterizes the statistical distribution of the local coercive fields and takes the grain size into account [2].
In recent studies it has been observed that the hysteresis losses of high-alloy silicon-iron laminations and other alloys do not really fit the first term in pFe in terms of the flux density squared dependence. This introduces a further adaptation coefficient α, which is usually between 1.6 and 2.2 for ferromagnetic materials and alloys. The inclusion of this factor leads to the following equation, which is now also commonly used in the post-processing calculations of finite element software, either with α = 2 [3] or a variable α [4], [5]:
It has to be noted that the presented loss separation approaches does not hold if the skin effect is not negligible [6]. A study on the properties of the coefficients from Bertotti’s statistical model is presented in [7].
Note: At low frequencies, the hysteresis terms are dominant, as expected. Frequency is a recurring difficult box. An article that should get this question out of the way for Steinmetz losses can be found here: Example: Template-based tightly coupled electro-thermal induction machine design.
whereby ${Modified Steinmetz Rotor Excitation Frequency} and ${MagneticFluxDensityinRotor.RotorCyl[Radial]Peak} are taken from the Steinmetz monitor.
In the figure you can see the the total loss of the Steinmetz model on the left and that of the Bertotti model on the right side.
Using Simcenter SPEED, it is relatively easy to compare progression models and determine loss coefficients for different materials and frequencies. At the moment (11/2023) it is not possible to calculate the Bertotti loss coefficients with Simcenter E-Machine Design.
1. In Simcenter SPEED, navigate to the Steel database under Tools and then start the Database Editor:
2. Choose a material you want, view details via View and switch to the Losses tab. There you can display curves and compare them with other models of the same material or with other materials. Set the plot to Loss vs. frequency. If you select the checkbox at the bottom left Plot second set of losses, you can look at the curves resulting from the model for different frequencies and/or flux densities one after the other.
3. When you now navigate to the Bertotti tab you can identify the loss coefficients of the respective model and use them to calculate the iron losses in Simcenter STAR-CCM+.