Simcenter MAGNET Thermal provides four component parameters, including CompositeMaterialDirection, that can be used to effectively specify anisotropic thermal properties for stranded coils. However, a problem occurs in 3D when the strand direction inside a given coil component is not unique, for example inside a coil end-turn. There is a simple scripting solution to get around this limitation.
Simcenter MAGNET Thermal provides four component parameters, including CompositeMaterialDirection, that can be used to effectively specify anisotropic thermal properties for stranded coils. However, a problem occurs in 3D when the strand direction inside a given coil component is not unique, for example inside a coil end-turn. There is a simple scripting solution to get around this limitation.
The following steps should be taken: