Opcenter Execution Electronics IoT - MSS (Valor IoT manufacturing - Shopfloor) API calls for interlocking

2023-11-29T12:50:12.000-0500
Manufacturing Systems Solutions

Summary

Below you can find configuration option, for API interlocking calls.


Details

The WIP API enables to report the routing database (Quality Management Database) with WIP information, and to perform routing validations. - when you report WIP on specific station, this station has the option to run a 'CheckRoutingStatus
This means, that when you scan in specific machine, if that checkbox is set, it will send a REST call to check, if routing is correct and if this board can move forward. You can find more details regarding this option in: MSS REST API Reference Guide (siemens.com)

Image_2023-10-31_14-15-38.png
Image_2023-10-31_14-22-02.png
Other WIP settings, are also described in :MSS Machine Settings Reference Guide (siemens.com)

KB Article ID# KB000123161_EN_US

Contents

SummaryDetails

Associated Components

Opcenter Execution Electronics IoT (Valor IoT Manufacturing)