Valor Process Preparation
Nexim version 2.7 support in Process Preparation version 2310
2023-11-30T11:05:00.000-0500
Manufacturing Systems Solutions
Summary
Process Preparation release 2310 will now support the latest Nexim version, 2.7.
Details
Nexim version now contains new API and new licensing. Process Preparation version 2310 is required for communication with this version of Nexim. Along with the main 2.7 version, following patches should be applied:
2830_V2.7.0_Plan_Patch
2861_V2.7.0_Valor_NeximDataControl_Patch
2985_V2.7.0_Plan_Patch
Or any later patch release which contain the same fixes. These should be delivered by Fuji. Patches should be installed in above order. Please check your current Nexim dongle compatibility with this version from Fuji. Version 2310 also contains other improvements to the Nexim interface, such as performance improvements. Please refer to the release documentation for further information.
NOTE: With the new Nexim API, the ValorExternalMachineServer MUST also be upgraded to version 2310.