Insights Hub
Asset Attribute Calculation - OOTB asset type details
2023-11-08T11:51:04.000-0500
Applications
Summary
example of Asset Attribute Calculation based on OOTB asset type details using Asset Attribute Calculator
Details
Based on the out of the box (OOTB) asset type details (here), only these attributes, where "considered in calculation" equals to "yes", will be counted in UTS multiplied by the number they are used/instantiated.
For example, when creating a new asset as below:
three attributes will be counted. Same results are displayed also by using the Calculator (here):
In case the above example will be used twice (e.g. by creating two assets), then in total 6 asset attributes (3 attr. x 2) will be counted in UTS.
The other attributes, where "considered in calculation" equals to "no", will not be counted even if instantiated and used.