Capitalâ„¢ Capital Manager does not start. Error in log file: ORA-01017: invalid username/password; logon denied

2023-10-12T18:09:59.000-0400
Capital Signal Modeler Capital Device Modeler Capital Capital Harness Process Designer Capital Harness Designer Capital E/E Reporter Capital Connectors Capital Harness Costing Capital Dictionary Capital Cabling Designer Capital CostingXC Capital Systems Integrator Capital Component Manager Capital Harness Designer Modular Capital Logic Designer Capital Project Manager Capital E/E Publisher Capital Symbol Designer Capital Wiring Integrator Capital Access Manager Capital Work Instruction Publisher Capital Systems Architect

Summary

The Oracle DBA changed the password subsequently Manager is not able to connect to the database with the original default password. The Manager connection credentials must be updated with the new password.


Details

The connection credentials for Capital Manager to connect to Oracle are stored in the <Capital Install folder>\config\managerprops.xml file on the Manager server machine.

The Capital administrator needs to edit that file, find the element "dbconnection" for the Oracle driver and update the password value:

<dbconnection driver="oracle.jdbc.driver.OracleDriver" hibernateDialect="org.hibernate.dialect.Oracle10gDialect" initialconnections="10" maxconnections="60" password="manager" pool="C3P0" url="jdbc:oracle:thin:@localhost:1521:dev" username="system" waitifbusy="true"/>

Save the file and re-start Capital Manager.

KB Article ID# KB000122755_EN_US

Contents

SummaryDetails

Associated Components

Capital Signal Modeler