Capitalâ„¢ Essentials
When Capital Essentials main release 2308 is installed the Images folder isn't created.
2023-10-05T17:28:59.000-0400
Capital Essentials
Summary
The Images directory allows users to store images that can be added to designs. When Capital Essentials main release 2308 is installed the images folder doesn't get created, users are unable to add images to their designs.
Details
To resolve this problem in main release 2308, the user can manually create a folder named Images in the installation directory of Capital Essentials. The problem will be fixed in main release 2308 Update 2312.